(0)| 6/17/2024 7:11 AM | |
|
Joined: 2/15/2024 Last visit: 6/16/2025 Posts: 2 Rating:
|
Hello 0_Einstein, thank you for the reply. I tried to search the "PLCSim restriction list", but I can't find it. What I can do is to share the TIA installed software: Few months ago I installed the "S7-PLCSIM_V18_SP2.iso", otherwise I wouldn't have been able to simulate with TIA Portal v.18. I tried to serch for some detailed information about SP2, but I only found this page: Readme_enUS_en-US.pdf - SIMATIC S7-PLCSIM V18 SP2 Readme - ID: 109823433 - Industry Support Siemens, where there are no much information to consult. So, I don't know if the PLCSim I have, is enough to allow the two PLCs in the project to communicate. To answer to your last question, I attach the configuration that is the same for both PLCs: |
| 2/17/2025 9:10 PM | |
|
Joined: 8/22/2014 Last visit: 8/7/2025 Posts: 87 Rating:
|
Hi, i also tried to use plcsim v18 in a project with put/get and two cpu. but simply not communicate. is it possible? tnz |
Follow us on