7/17/2006 6:58 PM | |
Joined: 1/7/2006 Last visit: 11/17/2023 Posts: 2705 Rating:
|
[quote user="Aero"]I recieve a new CPU (319-PN/DP) and want to load it, the first time, with Ethernet connection. Hi Aero, From Step 7 hardware configuration you may give in all the equipment around the CPU 319. After you have given in all equipment you may go online by the next menu-point from thedropdownmenu PLC --> Ethernet --> Edit Ethernet Mode, after search,there you can give in the information such as IP-address and so on, after that write it to the CPU319 andafter that you may directly load the hardware... [;)] The search is finding all equipment that could answer on the layer 2 protocol DLC (only Siemens equipment on Ethernet/Profinet). It is also possible to give the IP-addresses. There is also a tool on the Siemens pages that might be used, it is very easy to use and can be downloaded from the next link: Primary Setup Tool (PST) Version V3.1 Adress Setting of SIMATIC NET Industrial Ethernet Products [8)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on