11/23/2009 7:46 PM | |
Joined: 11/10/2009 Last visit: 7/30/2024 Posts: 1 Rating: (0) |
I'm having problems migrating the WinCC v4 -> v5. The attachment says it all. After migration started to have problems with data type STRING. In the example I / O Field should return the characters' PE80 ', but I only returns the characters '80'. I noticed that the first two bytes did not appear because they represent the size of STRING. I believe that the data type STRING are treated differently in WinCC V4. The question is, why it works in WinCC v4 and v5 does not work? I followed all the procedure for migration, also have made the process several times and the result was the same. Someone has been there. Sorry for English.
AttachmentERRO WINCC.pdf (37 Downloads) |
Follow us on