6/4/2010 10:34 AM | ||||||||||
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Tomy, Every CPU has an integrated PROFINET port, which supports standard PROFINET communications. The supported Ethernet protocols are described in the following two connection types:
More about RFC1006 and TCP protocol look in SIMATIC S7 S7-1200 Programmable controller. (Configuring the TSEND_C instruction transmit (send) parameters.... Best regards, Hristo Mihalev |
|||||||||
This contribution was helpful to2 thankful Users |
Follow us on