6/5/2010 7:00 AM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi phantom, 1. for Modbus TCP/IP the block is already used for PCS7 Librery, Please Checked the Modbus TCP/IP Librery or this post so in that you have to change the block & to change the Block No. it is not simple as Step 7. 2. Please Checked & reply me 3. You are right but offically Siemens has not launch the Manual, As we have for the PCS7 V7.0. so we can checked the Step as per the Manual, & if we want to make New face plate how we can build ? 4. Right now I am using the SP1 so this one is not Problem. 5. In PCS7 V7.0 we have Group Error, which I am used for the interlock in the logic, but in New one I have to Used the OR block & then I have to used in Logic. are you agree with me or not. Please Reply me I want to know the Your View on this, |
Ammy |
|
6/7/2010 2:58 AM | |
Posts: 2661 Rating: (279) |
Hi Ammy, I saw your older post and I think you ran into the problem with FC60 CMP_R because you did not rewire according to the instructions in the manual (relevant page from manual attached), Overall I agree with you that every library should have unique block numbers but since the blocks are created by various departments/divisions in Siemens, it is as difficult as expecting the various members if the U.N. to agreeing on something! Which manual? Let me know. A new faceplate can be still made using the Faceplate Designer... I agree that the group error is convenient to have but the lackof it is not a catastrophic shortcoming (strictly my opinion). Regards AttachmentRenaming of Standard Functions.pdf (511 Downloads) |
6/15/2010 4:04 PM | |
Joined: 4/19/2008 Last visit: 9/3/2024 Posts: 1525 Rating: (159) |
Hi Phantom75, 1. If the PCS7 we are talk, then there should be Interlink between Various Department, or they have to think on which are block are used are not consider we have to used it, & this are created By Siemens so End person know the Siemens only not the relative Department or person, they have to must Consider this, or otherwise they have to provide the instruction for Rewiring & Conflict of Block. & which Block are conflict in my case it is the Basic Block in the Process which we are using. 2. I am Taking about the APL Block FacePlate Which was introduce in V7.1 If you have the APL Face Plate Designing Manual Please Share with me. 3. For Group error it is very help full to adopt in logic. I want to share the My view related to PCS7 new look with old version & new Function,
Bye... |
Ammy |
|
6/15/2010 11:14 PM | |
Posts: 2661 Rating: (279) |
Hi Ammy, In an ideal world there should be interaction between various departments and they should agree upon the various blocks for each department. But in the real world there are many difficulties for achieving this because of the ever changing nature of the libraries. Many libraries get updated, some get discontinued and some new ones added. It is very difficult to maintain rigid guidelines. Easier way is to alert the user of a conflict and provide instructions for rewiring. This is being done increasingly by various add-on product developers, an example is the attachment in my last post. APL Faceplates is a separate product with new type of faceplates. And the Faceplate Designer uses templates as described in the following FAQ: http://support.automation.siemens.com/WW/view/en/22539815 However it is possible to “adapt” the APL faceplates for your custom blocks. This is a matter of opinion. IMO, the APL design philosophy is a bit different…
|
Follow us on