7/30/2010 1:14 PM | |
Posts: 3609 Rating:
|
Import of a Technical Question of an User franxi1970 wrote: Good morning I don't succeed in printing a protocol in the printer of net. Currently the printed ones is inserted in a net workgroup, we don't have a server of net we don't have a Print server I have given the following formulations in the control panel: PCL Laser Network: 192.168.0.83 type of sheet A4 I don't even see the panel MP277 8" in the resources of net. You have some suggestion please. it stamps her I have to momentarily make a firm, for then not to lose too many days from the client that it is found to the foreign countries. If I launch the runtime on Pc the protocol him press very well and from the panel that it doesn't work Thanks |
7/30/2010 1:35 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating:
|
Hello, Did you check in What settings are to be made when connecting a printer to a Windows-based panel?. best regards |
7/30/2010 2:20 PM | |
Posts: 1 Rating:
|
|
7/30/2010 2:28 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating:
|
You are wellcome! |
Follow us on