12/12/2011 1:23 PM | |
Joined: 7/3/2011 Last visit: 4/27/2024 Posts: 81 Rating:
|
Dear All, In my new project having as per attached configuration. The 2 315 2DP cpu with software redundancy with MPI network and one ET200s. The redundancy CPU's having CP-343-1 lean module (6GK7343-1CX10-0XE0) in each stations. I have checked my project in software redundancy with MPI network sucessfully. I want to exchange some data between 2 redundancy CPUs to ET200S. I have tired to create S7 connection between CP 343-1 lean module with ET-200s but the connection could not established. Is it possible to exchange the data between the cp 343-1 lean modules in redundant system and ET 200s. AttachmentS7 Connection.pdf (152 Downloads) |
12/12/2011 2:02 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Hello, In which station did you try to create S7 connection? Check it THIS. Best regards, Hristo Mihalev |
12/13/2011 7:55 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating:
|
Yes, it is possible. Make the configuration in Et200S CPU. Best regards, Hristo Mihalev |
12/13/2011 8:09 AM | |
Joined: 7/3/2011 Last visit: 4/27/2024 Posts: 81 Rating:
|
Dear UMENCHO, I have tired to create the S7 connection and TCP connection between S7 CP 343-1 Lean Module to ET 200s But the attached errors was came. Please are you know regarding help me. Thanks and Regards Strongs AttachmentNew Folder.zip (70 Downloads) |
Follow us on