5/18/2012 1:53 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (306) |
Hello, You cannot make just a cable going from AUI (transceiver interface) to 10BaseT Ethernet (RJ45) without any electronic involved. AUI and 10 base Tuse different electric signals. A possibility is the Media Converter Scalance X101-1AUI which is intended to connect a bus using Transceivers (AUI interface) to twisted pair (RJ45) network. See the link to SCALANCE X101-1AUI: http://support.automation.siemens.com/WW/view/en/23282470 |
Best regards |
|
This contribution was helpful to1 thankful Users |
5/19/2012 10:13 AM | |
Posts: 2 Rating: (0) |
Thank you for your help, because of disponibility of materiel, I change completely the CPU to 416-2DP and the CP to 443-1EX20 with RJ45 Best Regards M. AMELLAL |
Follow us on