6/27/2012 10:29 PM | |
Joined: 2/5/2007 Last visit: 9/9/2023 Posts: 101 Rating: (10) |
Hi, A customer had a HDD-failure. He replaced the HDD and restored the system from a Ghost image. As far as I know the image should be up to date. Anyway, the OPC doesn't seems to have contact with the PLC. I've been trying to browse the M's and DB's via OPC Scout which reports quality "bad". I've also talked to Siemens Support in Sweden and we have treied everything so far without any luck. It seems to work as you can see in attached document. The document isn't from the customers system. It's from a test system i created today. But the principle is... The status is exactly the same at the customer. The thing that differs is that my test system has an 315-2 PN/DP where I configured Rack/Slot as 0/2. My customers system has a CP 343-1 mounted in Rack 2/Slot 5. I've tried to change to 2/5 and 0/0 but with the same lousy result. Any ideas? Best Regards, -- Daniel AttachmentOPC_Trouble.pdf (56 Downloads) |
7/16/2012 4:25 PM | |
Posts: 1547 Rating: (129)
|
Hello, the connection has to be configured with Rack/Slot as 0/2. What result gives a ping command? Compile again in Netpro and load PC-station and CPU ... |
Follow us on