11/1/2012 8:37 AM | |
Joined: 9/9/2011 Last visit: 4/11/2024 Posts: 15 Rating: (0) |
Hello, I have also question about using another modem.I do not have MD720-3 I try to use CE-X25Library with MC55i Terminal (CPU 1211C fw2.2;CE-X25 V1.2;TIA V11 SP2 UP3). Initialization of modem goes through OK. But when I try to send message, I get error 8070 "The message of the SMS could not be transferred". The input parameters are correct (double cheked). Does anybody can help with it? Mayby I should change something in "com" FB? Thank You in advance! |
Last edited by: O_Moderator at: 11/1/2012 8:00 PMnew subject after splitting from /tf/WW/en/Posts/58132#top |
|
Follow us on