12/21/2012 11:38 PM | |
Posts: 267 Rating: (24) |
Hello, the only way I know to communicate to KNX is via LOGO! 0BA7 (S7-communication via ethernet to LOGO!) and from there via the LOGO! COMMUNICATION MODULE EIB to the KNX bus. http://support.automation.siemens.com/WW/view/en/18968781 |
12/23/2012 8:45 PM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
Hello George.Petalidis, I'm not very sure about the solution. But I would also like to know the possibility of the same. You can open a Support Requestfor this case, so that the technical support can help. |
Like it? Rate it! |
|
Follow us on