9/12/2012 12:26 PM | |
Posts: 1547 Rating: (129)
|
Ok I'm sorry I didn't get that you didn't configured an IP until now... You can use this tool for example to do this: http://support.automation.siemens.com/WW/view/en/19440762 |
9/24/2012 12:39 PM | |
Posts: 26 Rating: (1) |
i connected to the switch and set an ip i attach here some pictures... link is "down" in ports 5 and 6. these are the fiber optic ports that are not communicating... "statistics" dont show any data flow on ports 5 and 6 any idea? thanks Attachmentcapturas.pdf (294 Downloads) |
Last edited by: rherrero at: 9/24/2012 12:40 PM |
|
9/24/2012 12:55 PM | |
Posts: 26 Rating: (1) |
i forgot the event log from log 1 to 9 where done by me from log 11 where there before me Attachmentevent log.pdf (228 Downloads) |
2/11/2013 8:08 PM | |
Posts: 2 Rating: (0) |
Thanks Rated X any update about last post from rherrero i have the same problem eactly ,, and i will be approciated if more recommendation . regards |
Follow us on