3/29/2013 7:14 AM | |
Posts: 19 Rating: (0) |
Hello, In my Project, S7-400H with CP443-1. ( As Server) is communicating with Yokogawa DCS(As Client).The system is double sided redundant. TheFirst CP443-1 in Rack-0 is communicatingwell, Error=0, Status=0, While the second CP443-1 in Rack-1 showing Error=1, Status=16#8304, I have assured that hardware is OK. How can I troubleshoot in this regards, Enclosed is the details of Network configurtaion, and CFC Chart Status Saad AttachmentError_description1.pdf (32 Downloads) |
Last edited by: O_Moderator at: 3/31/2013 4:49 PMnew subject after splitting from /tf/WW/en/Posts/85922#top |
|
3/31/2013 5:00 PM | |
Joined: 4/24/2009 Last visit: 8/20/2024 Posts: 2682 Rating: (135) |
Thread closed, because question is already published in the following thread S7-400H with CP443-1. ( As Server) is communicating with Yokogawa DCS (As Client) Best regards O_Moderator |
Follow us on