4/5/2013 1:22 PM | |
Posts: 3093 Rating: (323)
|
Hello dhirenaidoo, you did itthe right way: define bytes in the send DB and set these to the required HEX values. P_SND interprets all data in the send DB as HEX bytes, it does not care whether they are characters, integers or reals. Make sure, that the checksum is calculated correctly. When the communication partner receives a wrong checksum it won't answer! Regards, Kaulquappe |
4/6/2013 7:45 AM | |
Joined: 8/12/2011 Last visit: 3/12/2020 Posts: 11 Rating: (0) |
Thank you! That was what I needed, just some confirmation. It seems the CP340 is only sending out one byte every time I trigger the P_SEND. There must be something wrong with my config. I will play around and figure it out. Thanks again for your help! |
Systems Integrator - South Africa |
|
This contribution was helpful to1 thankful Users |
Follow us on