9/8/2013 4:29 PM | |
Posts: 25 Rating:
|
thank you very much.. it made me persevere on finding/acquiring a copy of our backup configurations. anyway, i have further questions, if you may. now i have the protool configuration for the op270 6", and i have tried to migrate it to wincc flexible 2008 sp2. i changed the device to oop277 6". executed regenerate, then i received a (0) errors and (650+) warnings.. i have tweaked some noncritical issues, but i dunno if the remaining warnings could affect the implementation of the project. pls check the attached file, an output list of the compiler. Thanks! Attachmentcompiler_warnings.zip (104 Downloads) |
9/9/2013 3:34 PM | |
Posts: 3037 Rating:
|
Hello, You can click with the right mouse on your warning and use the function "Go to" to the error place. Tweety |
Follow us on