7/26/2007 8:42 AM | |
Posts: 8 Rating: (0) |
Dera Nemo, Here is out last diag log captured from two WinCC Servers. And eachtime after reboot the server, we will clear the diag folder in order not to mixed up the data. TheWinCC server 1 was rebooted on 22 July 07 and 25 July 07. The diag log has captured the data between these period. Thanks for your help!! Best Regards, Kant AttachmentSRV_Diag.zip (410 Downloads) |
7/26/2007 2:22 PM | |
Posts: 1275 Rating: (123)
|
Hi Kant, There are some errors in your logs, specially for Server 1, such as: Server 1: 2007-07-23 10:23:46,968 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![PartnerServer]: CoCreateInstance for server "OPCServer.WinCC" on machine WINCC_SRV2_KCR failed, Error=80040154 (HRESULT = 80040154 - REGDB_E_CLASSNOTREG (Class not registered))") Check this thread. 2007-07-23 02:00:34,906 ERROR Connectionerror 1 "RTU_S425": Errorcode 0xFFDF 410E! For this one, check these FAQ's out: 1 and 2. 255,25.07.2007,04:10:55:734,1007008,4,,WINCC_SRV1_KCR,SCRIPT,EndAct Timeout 255,24.07.2007,04:59:43:531,1003015,4,Administrator,WINCC_SRV1_KCR,Alarm Logging,AlarmLogging is being overloaded with 2446 messages / 10 min. Server 2: 2007-07-25 04:10:54,453 ERROR - ChannelUnit::SysMessage("[OPC Groups (OPCHN Unit #1)]![PartnerServer]: CoCreateInstance for server "OPCServer.WinCC" on machine WINCC_SRV1_KCR failed, Error=80040154 (HRESULT = 80040154 - REGDB_E_CLASSNOTREG (Class not registered))") 2007-07-25 04:11:04,453 ERROR ..FOPCData::InitOPC CoCreateInstanceEx- ERROR 80040154 Also.. check this out. Best regards, Danielle |
Follow us on