11/8/2013 4:50 PM | |
Posts: 118 Rating: (11) |
Hi javigis, |
11/11/2013 10:35 AM | |
Posts: 12 Rating: (0) |
Hi Simfairy,
thank so much for attached document.
As far I know I am at this scenery:
-Configuration 1: RS485 connection with dialup connection via modem
-Configuration 3: Ethernet connection with dialup connection via modem
I still have the following doubts:
-End device A (PG/PC): do I need a “special” modem or just through my internet connection is possible?
- End device B: probably I will connect my S7-300 with my HMI panel through Profinet connection. But I am going to connect the TS adapter directly to the PLC through MPI. Am I in Configuration 1 or 3? Thank you so much. Attachment26662448_WAN_Access_V10_e.pdf (38 Downloads) |
Last edited by: O_Moderator at: 11/11/2013 12:36 PM |
|
Follow us on