12/15/2014 11:55 PM | |
Joined: 5/29/2013 Last visit: 5/21/2024 Posts: 100 Rating: (28) |
Hey members of the Forum I am making the SET30 configuration on a S7-1200. to communicate from the PLC via GPRS to a remote internet connected PC. Configuration:
I have used the Set30 Example file and that works well. Now i have built it into a program that my costumer would like to control remotely, and now I seem to have some problems with the TC_RECV function. Well some problemsit’s just not receiving at all. The only difference that i could find is that my CP1242-7 have 2 Hardware identifiers. I think I use the right one now because all the other functions are also not working when i use the other ID. I have put my configuration in the attachment JPG. Here you will find my complete project archived as a download: (V13 update 6) https://www.dropbox.com/s/1cmyldt9ye9tbpy/ProjectX.zap13?dl=0 What am I doing wrong ? |
Regards |
|
12/22/2014 1:39 PM | |
Posts: 1368 Rating: (126) |
Hello, as INTERFACE, you have to take the HW_ID from GPRS-Interface. So the ID you used must be correct. EN_R must be true, otherwise the TC_RECV is blocked. The ID must be the same as TC_CON. Do you get some STATUS value? Here is an faq, which could be interesting for you http://support.automation.siemens.com/WW/view/de/72550534 |
Follow us on