11/3/2014 7:48 AM | |
Posts: 17 Rating: (0) |
good afternoon all, my question is regarding downloding a program to IM 151 -8 PNDP pls to which Interfacing module is also attached. but i am unabe to download program, when i search accessible devices den my plc and im module are accessed but as soon i start do download configuratin it shows // target device can not b reached/// and by observation i found that when i put memory card in plc den plc goes in fault mode. ,,,,,,,,,,,so though after creating a big program m not able to download it,....what should i do now...to download program..
---------------------------------- New subject after splitting from TCP/IP Communication between S71200 and S7 remote CPU IM151-8 PN/DP. |
Last edited by: Min_Moderator at: 11/3/2014 3:00 PMSplitted |
|
11/6/2014 12:01 PM | |
Posts: 17 Rating: (0) |
can any one please help me in above matter.. |
11/6/2014 2:46 PM | |
Posts: 1058 Rating: (93) |
Hello pravins777, this has been discussed here already: IM151-8 PN/DP not downloading Problem downloading configuration from Primary Setup Tool (PST V4.1) to IM151-8 PN/DP CPU regards |
1/16/2015 7:58 AM | |
Posts: 4 Rating: (0) |
Pravin, I am also facing the same problem, how can i reset mmc thr simatic?
|
1/16/2015 8:05 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
How do you format or reset an MMC (Micro Memory Card) for SIMATIC S7-300 CPUs? |
1/16/2015 8:43 AM | |
Posts: 4 Rating: (0) |
By following your procedure I am getting continuous reset demand, I should replace the mmc . |
Follow us on