4/10/2015 3:33 PM | |
Posts: 1 Rating: (0) |
I have several RX1510s that have the first release of ROXII on them. I have gotten the latest release zip from the Siemens support and have attempted to follow the user guide to install it. I have setup a Windows Server 2012R2 instance with the IIS7 role. Under the default website I have extracted the zip file. I changed the mime file type just like the manual instructed. I serial connected to the devices and inserted the url http://192.168.1.254/ and the release as rr2. I receive an error the device can not apt-get the listing. The manual has not been very clear on how the file structure on the webserver needs to be listed and which release I need to instruct the device to obtain. Any help that can provided would be greatly appreciated. |
Follow us on