4/10/2015 10:26 PM | |
Posts: 14 Rating:
|
Hello, My default setting shows the same thing that I enter everytime to make an connection. I have a question. for setting up a PG/PC interface do I have to add the hardware in TIA portal or not. if not, then what is the procedure of talking to PLC via computer/laptop
look, I have this PLC 1515f 2PN, I need to talk to it. so I changed my Ethernet settings, I changed its IP address, then connected the PLC to Scalance, and Scalance to Laptop Via Ethernet cable. opened the TIA POrtal, >Online & Diagnostics> Portal View> accessible devices a pop up window came. it asked me type of the PG/PC interface: I selected PN/IE it also asked PG/PC Interface: I selected my Ethernet card in it. and pressed Start Search, the result was that " no accessible nODe were found. **when I try to ping my PLC from laptop, I doo get results from it. that its responding.
now help me what is it that I am doing wrong
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/13/2015 2:14:57 PMNew subject after splitting |
|
Follow us on