6/13/2014 4:45 PM | |
Posts: 5 Rating: (0) |
Hello, I'm facing the same problem related inSureshsai's post. I'm using a standard ethernet adapter (IE General). This is my hardware and software configuration: Server: HP Proliant DL388 G7 Windows Server 2008 SP2 WinCC 7.0 SP2 SIMATIC NCM PC 5.4 SP5 HF1 SIMATIC NET 7.1 SP2 I'm configuring the conection for my PLCs using the NCM and Station Configuration Editor. When I make the configuration of the station using command "PLC -> Configure": - Index 1 (OPC) is started without problems - Index 2 (IE General) don't go to RUN status. After making the configuration, I'm trying to do the download with the command "PLC -> Download" and the station is not found, but my network adapter is ok. I'v already tried to make a lot of tests, including UMENCHO's sugestion. I've seen this problem in other applications. Is it a known problem of SCE? Could anyone help me? Thanks.
|
7/4/2014 12:59 PM | |
Posts: 5 Rating: (0) |
Hi, This problem was solved reinstalling NCM and SIMATIC NET.
|
This contribution was helpful to1 thankful Users |
2/29/2016 3:58 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by fdsf is split to a separate thread with the subject Station configuration editor, Add button is diabled. Best regards |
Follow us on