3/20/2012 9:41 AM | |
Posts: 1547 Rating:
|
Hello Silvio, |
This contribution was helpful to
1 thankful Users |
3/20/2012 9:59 AM | |
Joined: 10/7/2010 Last visit: 7/8/2024 Posts: 103 Rating:
|
thx u Rated X! |
3/26/2016 4:08 AM | |
Joined: 7/30/2015 Last visit: 2/8/2023 Posts: 3 Rating:
|
I do not see the HMI port designation on this document. Port 102 will just get me to the PLC, what port can I forward through my router to reach a Siemens HMI? The particular one I am working on at the moment is a TP900 Comfort but I expect all the Siemens HMI's use the same port. Also, can the port on the PLC or the HMI be altered? If I am trying to access remotely through a router to more than one PLC without using a VPN I need to forward ports to the respective PLC. Can these be changed? Thanks. |
Follow us on