3/31/2008 1:37 PM | |
Posts: 4 Rating: (0) |
Hi, In the PC Sever I've created a share folder with name "prueba" and I give all permiss to the same user that I configure on the Network ID on the MP277. From another PC,using this user andthe same IP address configured, I connect to the shared folder on the PC Server whithout problems. But if I try to connect to PC Sever from MP277 I get the message that path is incorrect. (you can see this on error.jpg). If the runtime starts in the diagnostics buffer I get the error number 80015 "the system cannot find the drive especified". Attachmentimages.zip (235 Downloads) |
3/31/2008 2:23 PM | |
Joined: 9/1/2005 Last visit: 9/18/2024 Posts: 4104 Rating: (195) |
closed cause question posted twice. The second thread with the subject Archive data with MP277 on a shared folder is published within the conference SIMATIC WinCC flexible. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on