8/25/2016 7:43 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (820) |
Hello, look to this topic with sample project. Project is working with RS-232 CM module but can be implemented with RS-485 HW. Your RFID device can be on other side like this Hyperterminal PC application. Look for first to RFID communication settings, you need set same on your PLC HW for proper communication. Look also to RFID documentation about messages you need send/recv to/from RFID device to receive needed data. Sample program S7-1200 RS 232 ASCII HyperTerminal comunications Update: in case of not misunderstanding, you've ask that you have same question, it means that your RFID device communicate via Modbus? I see your point to point info, but you have post this on topic about Modbus ASCII, therefore I ask for sure. Pls create your own topic next time because this can be chaos for others. Can you confirm this, better explain your info again for sure? |
Last edited by: Duris_I at: 8/25/2016 10:05:41 AMLast edited by: Duris_I at: 8/25/2016 10:06:19 AMWith best regards... |
|
Follow us on