2/20/2017 7:51 PM | |
Posts: 1 Rating: (0) |
Boa tarde, foi atualizado o catálogo de hardware via internet e não foi atualizado o catálogo da CP 6GK7343-1CX10-0XE0 de versão 3.1. O equipamento é novo. Tem algum lugar que possa solicitar esta atualização especifica? ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/21/2017 9:31:45 AMNew subject after splitting |
|
2/21/2017 7:54 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi RonaldoRibeiro, this is an english-speaking forum. If you want others to help you, write englisch as well From Google-Translator:
Regarding to your question: The 6GK7343-1CX10-0XE0 has no FW 3.1 as you can read on the product-page on SIOS the last Versions are: VersionsE version: HW: 07Firmware version: FW: V3.0.23Software version: COMMUNICATION PROCESSOR CP 343-1 LEAN hope this helps, regards, |
FCK WAR! |
|
3/15/2017 5:12 AM | |
Joined: 11/16/2016 Last visit: 6/28/2022 Posts: 1 Rating: (0) |
I have the CP 343-1 Lean and on it stays V3.1. Additional - i have downloaded extra the firmware 3.1 for CP343-1 Lean (CP3431CX10_V3.1.1), but it doesn't help me... The same question - why I cannot see it online, when its configured in TIA V13 SP1 as V3.0. How I can update the catalog in TIA? EDITED: I found that the CP-343 firmware 3.1 is released Entry date:05/02/2016 Info. I read and tried to update the catalog information in TIA, but it says the module is up to date.. |
Last edited by: AutoGen_6592643 at: 3/16/2017 3:51:32 AM |
|
Follow us on