12/30/2016 4:52 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, Citec can be OPC Client and other OPC Clients could reach the same symbols. Citec would play the role of the PC (being OPC client). For the new S7-1500 PLCs, as of FW 2.0, the OPC server can be run in the PLC itself. |
Best regards |
|
This contribution was helpful to1 thankful Users |
1/2/2017 12:27 PM | |
Posts: 2 Rating: (1) |
Hi jklm, Thanks a lot for that! Can InTouch use the same OPC server talking to S7 300/400 for symbolic addressing? |
1/2/2017 4:50 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, |
Best regards |
|
3/20/2017 11:22 AM | |
Joined: 3/21/2006 Last visit: 10/7/2024 Posts: 10229 Rating: (1181)
|
Intouch OPC Client is called OPCLink. Can read from any OPC server. BR |
Follow us on