5/19/2017 11:13 AM | |
Joined: 11/17/2010 Last visit: 9/12/2024 Posts: 216 Rating: (40) |
Hi, I tryed to read port diagnostic of scalance X204-LD thru CP343-1 but SFB52 return error 16#C0809000. I tryed the same block and code when scalance is linked onto integrated PN port of the CPU and it works. I used the document attached to create the code. I'm using : Step 7 V5.5 CPU 317F-PN/DP CP343-1 (1EX30) Scalance X204-2LD. Any ideas ? Regards. AttachmentRead diagnostic of Ethernet port (SFB52).pdf (78 Downloads) |
Follow us on