7/20/2017 11:50 AM | |
Posts: 13 Rating: (1) |
Up! Of course you are right. But now i did some experiments and had seen interesting things: My soft - TIA v13 SP2 Hard: CPU 1513-1 PN 6ES7 513-1AL01-0AB0 v2.0 and CPU 315-2 DP 6ES7 315-2AG10-0AB0 V2.6 and CP-343-1 6GK7 343-1EX30-0XE0 I create - on the 1500 cpu side: GET and PUT on the 300 cpu side: GET and PUT_S. I have the Error status 27 on the GET block, but it works. I realize the hartbit exchange between two cpu, and it works. If I use PUT block - not work. Data is not sent. Maybe this be helpful anybody ---- sorry if my english is not good ------------------------------------------------------------------------------------------ |
Last edited by: anchi at: 7/20/2017 11:56:14 AMLast edited by: Jen_Moderator at: 7/21/2017 1:42:11 PMNew subject after splitting |
|
Follow us on