8/11/2017 10:03 AM | |
Joined: 10/17/2011 Last visit: 7/19/2022 Posts: 148 Rating: (3) |
Hi, I have 6ES7 137-6AA00-0BA0 CM PtP communication module on ET200SP remote station with CPU 11517-3PN/DP I am using it for Modbus Rtu communication with Energy meter EM6400. On energy meter , I can access only these parameter settings: Data Transmission rate: 19200(we setas 19200) Parity: we set as Even we are not able to access Data bits and Stop bits settings on energy meter. But in manual we found it as Data bits:8 and Stop bits:1 at PLC end we did hardware settings as: as shown in attachment I am not able to read any values ike current, voltage or frequency from energy meter Please let me know, where it is going wrong. I have connected Data + from energy meter to Terminal 12 on CP module and Data - to terminal 14 on cp module. Thank you, Damayanti ------------------------------------------------------------------------------------------ Attachmentmodbus.zip (29 Downloads) |
Last edited by: Jen_Moderator at: 8/11/2017 2:09:40 PMNew subject after splitting |
|
Follow us on