12/27/2017 8:36 PM | |
Joined: 9/27/2006 Last visit: 8/7/2024 Posts: 12273 Rating: (2680) |
Hello geri; Of course you can use the S7-1200 controllers with distributed I/O systems, whether from Siemens (ET 200M, ET 200S, ET 200MP, ET 200SP....) or from other manufacturers, such as Wago, Weidmuller and others. Easiest is using the integrated Profinet port on the S7-1200 controller for distributed I/O connection. You can also add a Profibus master (CM 1243-5) to the S7-1200 rack so you can setup remote I/O on Profibus-DP just as easily. For a good presentation on distributed I/O with the S7-1200, have a look at the video and documents from this link Automation tasks in 10 minutes- S7-1200 distributed I/O Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 12/27/2017 8:37:51 PM |
|
This contribution was helpful to1 thankful Users |
12/28/2017 3:10 PM | |
Posts: 152 Rating: (5) |
Thank you very much, this was really helpfull! :) |
12/29/2017 1:05 PM | |
Joined: 9/1/2005 Last visit: 8/1/2024 Posts: 4104 Rating: (194) |
closed cause question posted twice. The second thread with the subject 1214 DC/DC/DC with distributed I/O is published within the conference Communication / Networks Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on