1/20/2018 3:31 PM | |
Joined: 7/8/2012 Last visit: 3/24/2022 Posts: 13 Rating: (0) |
Hi Murof, Details as below, HMI Device : WinCC PC station (with CP5612) Version of TIA Portal : WinCC RT Professional V13 PLC Device : S7-1200 1214C DC/DC/DC with CM1242-5 (Profibus slave) Firmware Version of PLC : V4.1 Image Version of HMI : 13.0.1.0 Issue : Cannot make connection/communication b/w PLC and WinCC Screen shots of Devices and Network view are attached. Thank you for the support. AttachmentWinCC_RT+S71200.zip (128 Downloads) |
Follow us on