4/6/2018 1:57 AM | |
Joined: 4/4/2018 Last visit: 6/2/2023 Posts: 3 Rating: (0) |
I am trying to communicate a HMIGXU3500 (Schneider) and a S7-1200 through RS-485 (CM1241 module), with the protocol MODBUS RTU. The HMI is working as a master, the cable connection is the following: CM1241 HMIGXU3500 3 2/7 8 1/3 5 5 No terminations resistors. I configured the MB_COMM_LOAD, no erros, and MB_SLAVE no erros, the RX led blinks, but the TX led not, and there is an communication error in the HMI, What am I doing wrong? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/6/2018 9:54:19 AMNew subject after splitting |
|
4/6/2018 1:47 PM | |
Joined: 4/4/2018 Last visit: 6/2/2023 Posts: 3 Rating: (0) |
Hi! Here is the image of my program attached. AttachmentS7_1.pdf (90 Downloads) |
Follow us on