4/14/2018 1:35 PM | |
Posts: 1 Rating: (0) |
hello, i have the same problem can u help me pls i am new in the world of automation and i am working on a personal project where i need to connect via ethernet a plc siemens s7 1200 ( where i put my main program ) and arduino. the sensors and electrovalves are connected to arduino card, and i want to manage them from the s7 1200 how can i send instruction to open the electrovalve from the s7 1200 to arduino when the soil is dry i need what to do that ? in the plc and in arduino i can use tsend_c trcv_c or put and get ?? what i need to do in arduino help me pls thank u ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/16/2018 10:39:15 AMNew subject after splitting |
|
4/16/2018 12:27 PM | |
Joined: 8/3/2009 Last visit: 10/18/2024 Posts: 13982 Rating: (1760) |
Hello I found this one with google: http://settimino.sourceforge.net/ perhaps this is what you are looking for. bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on