5/31/2018 10:46 PM | |
Posts: 1 Rating: (0) |
We need to change the way the TIM card responds when a general poll (i.e. a Class poll or any variation poll) is sent by the Master. As it is set now, it will respond with 32 bits analogs values. To be properly processed by our Master, it has to be 16 bits. On page 38 of TIM 3V-IE DNP3 Complete Device Profile document, it is indicated that the default variation can be changed by loading a "proprietary file via other mechanism". Where we could get this file, and where we could get instructions for loading this file. An extract of the referred page is attached, to help in the explanation of this question. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/1/2018 1:28:29 PMNew subject after splitting |
|
Follow us on