6/27/2018 11:20 AM | |
Posts: 3 Rating:
|
Hi all, I'm trying to do a S7 PUT from a S7-1512 to a IOT2000EDU software PLC via the TIA portal. Attached are the screenshots of the project in TIA portal. I have the PUT block as part of OB1 in S7-1512 and its trying to put the data field "RuntimeMeasurement_DB.MeasuredRuntime" to "DB_RECV.time" in the IOT2000EDU. And this is not working. I don't see the value in the IOT updating nor do I see S7 communication when I do a packet capture in Wireshark. A few things I noticed: 1. One of the S7 communication links under Devices and Networks shows "exists only offline" in the TIA portal. How do I persist this link to the device? 2. I wasn't able to find a flag in IOT2000EDU to enable PUT/GET similar to S7-1512. Is there something like that? Any help is appreciated. Thanks AttachmentPics.zip (25 Downloads) |
6/29/2018 10:19 AM | |
Posts: 3 Rating:
|
Thanks for your reply. Which config error are you referring to? |
6/29/2018 10:29 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating:
|
Hello, check attachment pls. |
With best regards... |
|
Follow us on