6/30/2018 9:49 AM | |
Joined: 8/10/2009 Last visit: 5/19/2024 Posts: 166 Rating: (2) |
Dear User's , Will there be a BUS FAULT : If there are two CP 343-1 Lean in one network and the Object name is same but different IP's : 1st CP : Name : cp-343-1-lean Mac Address : 00-1B-1B-39-39-A2 IP Address : 10.1.41.11 Subnet Mask : 255.240.0.0 2nd CP : Name : cp-343-1-lean Mac Address : 00-1B-1B-37-C9-60 IP Address : 10.1.26.11 Subnet Mask : 255.240.0.0 Both the IP's are pinging from the laptop being in the same network . [snip] Thanks Sarabjot Singh Manku [snip] AttachmentDiagnostic buffer of module CP 343-1 Lean.txt (33 Downloads) |
Last edited by: ssmanku1699 at: 6/30/2018 9:50:25 AMLast edited by: Jen_Moderator at: 7/2/2018 10:15:48 AMAdded diagnostic buffer as an attachment and deleted phone number, because doesn't comply with forum terms. |
|
Follow us on