8/14/2018 2:13 PM | |
Joined: 8/30/2009 Last visit: 1/20/2021 Posts: 41 Rating: (0) |
Dear All, I've got some strange situation: KTP700 panels can not correctly show circles and squares. Tested on TIA14, TIA15. Tested on one KTP700DP and two KTP700PN (2nd gen). AttachmentKTP700_geom.zip (39 Downloads) |
8/15/2018 11:49 AM | |
Joined: 8/30/2009 Last visit: 1/20/2021 Posts: 41 Rating: (0) |
Hello! Circles and squares are from Toolbox - Basic objects. Properties "Fill Pattern = Transparent" and " Border Width = 2" were changed only to show the figures better. To make photos, I've developed a new screen in a new project. With new circles and squares. Photos are made from KTP700DP. As you can see, in develope environment and in simulation the geometry is well. But in panel runtime the geometry is wrong. Also this effect one can see on Transfer screen of KTP700: the indicators PROFIBUS and USB are not round, but they must be. This thing was detected on KTP700PN on another project after download to device. Tested on two KTP700PN panels, on TIA14 and 15, on three different projects, without COPY-PASTE. AttachmentIMG_20180815_123528.zip (27 Downloads) |
Follow us on