8/21/2018 1:42 PM | |
Joined: 8/12/2011 Last visit: 2/11/2024 Posts: 20 Rating: (0) |
Hi, Here I attached the project and connection details Is there any possibilities to give the gateway to S7-1200 CPU AttachmentModbus OVERVIEW and Details.docx (366 Downloads) |
8/25/2018 10:17 AM | |
Joined: 8/12/2011 Last visit: 2/11/2024 Posts: 20 Rating: (0) |
Hi Find the attached document, Iam using MB_server to send data through the ModSim the data send and receive no issues. While connect to MOXA at receiver end the data not receiving AttachmentBlock diagram MOXA.docx (242 Downloads) |
8/25/2018 2:23 PM | |
Joined: 8/12/2011 Last visit: 2/11/2024 Posts: 20 Rating: (0) |
Hi, As you said I tried but not working, I have gone through Another setup Explained below 1. With Two 2 nos CPU-1500 i checked the Mod-bus communication as MB_server and MB_client the connection work fine but when i Connect the MOXA GSM device G3150 it is not working 2. During the Moxa G3150 (GSM) connection in between two CPU 1200 PLC Configuration below MASTER CPU 1200 IP Address:- 192.168.0.100 MODBUS (MB_Server) partner IP :- 192.168.0.20 (THE Moxa Ip is Partner IP) CLIENT CPU 1200 ip Address :-192.168.0.18 MODBUS(MB_Client)partner IP :- 192.168.0.10 (THE Moxa Ip is Partner IP) This configuration will work or not most importantly MB_Server and MBClient will work or not, if any other block let me know Find the Attachment for more info Regards AttachmentBlock diagram MOXA.docx (127 Downloads) |
Follow us on