10/1/2018 8:57 PM | |
Joined: 10/9/2017 Last visit: 6/20/2024 Posts: 9 Rating:
|
I've a problem with trying to use InTouch to connect to one of our machines. Its a cnc machine with a Siemens NCU 720.3 which contains a 317-3 PN/DP. This worked until the NCU failed and had to be replaced but now can't get a connection in intouch to the PLC. The only difference between this machine and one thats working is in the communication tab of the module information. S7 communication Occupied is not set and other communication isn't set to 3 like the other machines. I've looked through the hardware and network config but I can't see anything missing. Can someone point me in the right direction? Ive uploaded 2 screenshots
Attachmentshaunzer.zip (20 Downloads) |
Last edited by: The Helping Hand at: 10/2/2018 2:24:55 PMDeleted link, added Zip-File |
|
Follow us on