10/12/2018 7:21 PM | |
Joined: 10/15/2015 Last visit: 7/11/2024 Posts: 7 Rating: (0) |
Hi Gents I've the same problem on two different Laptop, with WIN10 OS with different VM, Go online with PLC and after 30 sec communication fail Both with TIA14 and 15, connecting with 1500CPU (didn't check 1200 but with 300 communication is ok) I remember similar problem communicating with CU of S120 I try different settings with VM (bridged auto or not, etc...) but problem still exist Every helps is glad for me Thanks ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 10/15/2018 7:51:33 AMNew subject after splitting |
|
10/15/2018 12:35 PM | |
Joined: 8/3/2009 Last visit: 9/18/2024 Posts: 13728 Rating: (1728) |
Hello do you have installed the latest Update? https://support.industry.siemens.com/cs/ww/en/view/109755826 Disable anti Virus scanner and Firewall on Host and VM for testing. Try to connect with a direct cable not with Companies network switch. Bye Murof |
Last edited by: Murof at: 10/15/2018 12:36:43 PMIf this Information really helps, you could use the Rate function |
|
Follow us on