12/6/2018 7:28 PM | |
Posts: 2 Rating: (0) |
I have a similar issue with S7-1200 communicating with multiple (4) devices over UDP using TRCV_C block. Currently I'm using one TRCV_C block to recieve data on port 2000, and if I exceed about 30 packets per second, the data seems to buffer causing a delay. If I create separate TRCV_C blocks, can I receive more packets per second on port 2000? If not, can I use separate port numbers to receive more packets per second? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/7/2018 10:19:44 AMNew subject after splitting |
|
12/7/2018 7:04 PM | |
Posts: 2 Rating: (0) |
Should these separate connections use different port numbers or can they use the same port? |
Follow us on