12/20/2018 11:30 AM | |
Posts: 7 Rating:
|
I have to connect a server PC to S7-400 PLC through ethernet. I used Open communication Wizard for Industrial Ethernet for configuring the IP address of the host (PLC) and the server PC (which is from other company). In the PLC Port address 1500 is used and which port address should I use for the PC. In a similar system which I saw, they have used the port address as 1266, and I tried with the same address but it doesn't work. How else I could find the port address of the PC system to communicate with the PLC. I selected TCP native as its S7-400 PLC and passive communication as the PLC doesn't need to send the data back to the server system. Regards, Rajesh. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/20/2018 1:49:35 PMNew subject after splitting |
|
Follow us on