2/6/2020 10:47 PM | |
Joined: 12/22/2015 Last visit: 5/15/2023 Posts: 3 Rating: (0) |
Hello, I have the same problem, I want to connect s7-1214C as profibus Master. I downloaded GSD file, and in this file there are modules: 6ES7151-1AA03-0AB0, 6ES7138-4CB10-0AB0 6ES7131-4BD00-0AA0, 6ES7135-4GB00-0AB0, 6ES7132-4BD00-0AA0 I see this modules in GSD, but I see also modules that Sarmiento have in earlier. So it should work? Or how can I check that modules I have are to old? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/07/2020 10:16:56New subject after splitting |
|
3/4/2020 11:44 PM | |
Joined: 12/22/2015 Last visit: 5/15/2023 Posts: 3 Rating: (0) |
Hello Murof, I have TIA Portal V13 SP1, cpu: 6ES7214-1HG40-0XB0; Profibus module : 6GK7243-5DX30-0XF0 |
Follow us on