9/19/2006 1:16 PM | |
Joined: 4/24/2006 Last visit: 6/28/2024 Posts: 8698 Rating: (1160) |
Hello, Have you seen the following faq: http://support.automation.siemens.com/WW/view/en/17413251 Hope this helps Best regards, Wizard |
This contribution was helpful to1 thankful Users |
9/23/2006 1:56 PM | |
Posts: 102 Rating: (9) |
Dear Chris Thanks a lot. Now I can browse The OPC server in OPC scout. But when I want to add items I got this error message: The item definition does not exist in the server address space. I have attached my symbol file. Address of “1” is: DB1.DBX1.0 Address of “m00” is: M0.0 I have DB1 in my s7 project and it has 6 bytes. Thanks, Mehrnoosh AttachmentUntitled2.zip (533 Downloads) |
6/12/2020 4:08 PM | |
Joined: 8/21/2014 Last visit: 6/28/2024 Posts: 971 Rating: (13) |
New question published by Pak Liam is split to a separate thread with the subject can't download to OPC server from simatic manager. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on