7/4/2020 10:25 AM | |
Joined: 3/21/2019 Last visit: 2/14/2022 Posts: 1 Rating: (0) |
Hi to all. Can i use getput block using cm 15242-1? Thanks |
7/6/2020 7:44 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi Gilbertz101, the module CM 1542-1 supports the S7 communication so you can use the functions PUT and GET. With regards |
7/6/2020 8:47 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (821)
|
Hello, manual: CM1542-1 Manual From manual is clear that S7 communication is available via ISO on TCP. What exact blocks you can use (S7 communication is wide area not only PUT/GET) you need check inside TIA communication library what blocks you have there available. On other side, what communication blocks you need use also depends to what comm partner you need create connection. What exact role it can play (Client/Server) you can check maybe inside TIA HW catalogue about description of CM. |
Last edited by: Duris_I at: 07/06/2020 08:53:08Last edited by: Jen_Moderator at: 07/06/2020 12:46:05Optimized link. With best regards... |
|
Follow us on