7/16/2020 12:01 PM | |
Posts: 66 Rating: (1) |
Hello everyone, i need a help with an issue i am facing with establishing data exchange between to master PLC's where they share only same IP network 1st plc is 168.192.0.102 2nd plc is 168.192.0.42 the both PLC's meet only on ethernet thru a switch the two plc are in different programs as i you can see in picture each plc has it is own hardware configuration, each plc represent a production line ( the 2 plc are not on multi project ) However, i tried to use fb34 GET_E for Awazil project (see in picture) to receive some info from GS_PROD but i could not establish that as you can see in pictures since it is not a multi project so when i did the communication settings i choose unspecified in connection partner local ID i used it in my FB34 block ID as W#16#A050 but still communication is not established AttachmentNew WinRAR ZIP archive.zip (51 Downloads) |
Follow us on