5/7/2019 1:16 PM | |
Joined: 8/3/2009 Last visit: 11/5/2024 Posts: 14087 Rating: (1766) |
Hello Heisenberg95 connect directly to the PLC with your engineering PC and set a fixed IP in the same Subnet as the PLC is. Then use the TIA Portal or the TIA Automation Tool (LINK) to set the IP Adress to the new subnet. after this change you have to change also the IP Of the engineering Station to the same subnet. Bye Murof |
Last edited by: Murof at: 05/07/2019 13:17:14If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
5/7/2019 3:33 PM | |
Posts: 37 Rating: (0) |
Can you be more explicit please ? And is there a detailed guide to do it ? |
5/13/2019 10:41 AM | |
Joined: 8/3/2009 Last visit: 11/5/2024 Posts: 14087 Rating: (1766) |
Hello If you have IP Adress conflicts and you do not know where or which Device produces the error you can use an IP Scanner to check the Subnet like this one (LINK) Bye Murof |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on