7/27/2020 2:17 PM | |
Joined: 5/13/2020 Last visit: 11/14/2023 Posts: 1 Rating: (0) |
Hello Christoph, When I try running both IRT and RT on the same bus I get an update time error 'no update time can be calculated for IO device', this is with the RT devices being listed as unsynchronized. Is there anything that can be done to rectify this? Is it possible to create two sync domains for one CPU? One sync master the other an unsynchronized domain? Thanks! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/28/2020 06:39:07New subject after splitting |
|
This contribution was helpful to1 thankful Users |
Follow us on