8/14/2020 12:02 PM | |
Posts: 3 Rating:
|
Solutions...?? |
8/15/2020 8:09 AM | |
Joined: 9/3/2008 Last visit: 7/7/2024 Posts: 926 Rating:
|
Hi, If you have the two cpus in the same project and make the S7 connection between the cpus, then make sure you download to both cpus so the S7 connection information is downloaded to both cpus. If you have the cpus in different projects, then in one cpu, you only need to enable the allow put/get option and the other is the one where you call the put/get and create the unspecified S7 connection. Also make sure the DB areas in both cpus are non-optimized. Then it is a matter of the program logic that calls the put / get. See the FAQ 82212115 for a description of this. |
Michael |
|
Follow us on